Success Stories

Keeping BMC Customers Safe on the Road

Quality bikes, from children's to downhill, are BMC Switzerland's core. Previous fasteners didn't meet customer demands. A new bolt with a built-in safety function, developed by Bossard and BMC, now greatly enhances cyclist safety.

Three men dressed in red and black jerseys with BMC logo cycling together, highlighting their shared passion for biking.

Screws: An Overlooked Component in Bicycle Manufacturing

BMC Switzerland may not yet be one of the big bicycle manufacturers. But that is what makes the BMC (Bicycle Manufacturing Company) strong: They are a small customer-oriented company with its headquarters in Grenchen, Switzerland, whose goal is to bring joy with high-quality bicycles. BMC stands for Swiss quality, which the company demonstrated with strong performances of the racing team in the Tour de France, becoming a world-renowned bicycle manufacturer.

The high demand for quality and precision is already evident when Development Manager Stefan Christ speaks about the diverse challenges in producing a bicycle. "In internal and external stress tests, it's often the screws that don't withstand the extreme stress," he explains. Not because they are of poor quality, but because this important element often receives too little attention.

Screws are often the components that are a hard nut for us. Whether screws or other connecting elements, they are critical points in the structure of the bicycle and can greatly affect the safety when riding.

Stefan Christ, BMC Development Manager

Engineering Aesthetics and Durability

Another focus of the high-tech bicycle manufacturer is design. A BMC bike should stand out from the crowd even without color and logos. This requirement presents another challenge for the engineers who are searching for the ideal fastening solution. Typically, the screws must be coated black so that they match the unified quality look and feel of BMC. Additionally, the wheels must withstand the harshest requirements in standardized stress tests in terms of vibration and corrosion. Only when the lightest screw with the best cost-performance ratio is found, the solution will be ideal.

ecosyn® grip screw on white background

Developing a Specialized Bolt for Optimum Performance

For this use case, Bossard has developed ecosyn® grip, a specialized bolt that meets both client-specific requirements and the standard regulations of EN14766 for mountain bikes.

EN14766 consists of a comprehensive set of safety regulations for bikes and the accompanying test methods to ensure their quality and performance. The standard requires that the handlebar and stem must endure 200,000 cycles during an endurance test, making it a stringent test of the materials and components used. In response, Bossard conducted a thorough analysis of the existing design and various tests to evaluate the mechanical properties and behavior under vibration.

Meeting Highest Industry Standards

ecosyn® grip meets the high demands of the bicycle industry for quality, precision and safety. This bolt is a testament to our commitment to providing reliable and high-performing products for the industry. BMC's interest in the performance of the newly developed bolt led to an extensive endurance test. Over the course of a month, the bolt was subjected to over 4,000,000 pedal turns under high vibrations and harsh environmental conditions to gauge its quality and performance.

Tested for Enhanced Safety and Performance

The results of the tests were overwhelmingly positive and confirmed the high quality of the bolt. To ensure the accuracy of the results, the tests were not only conducted in the company's own facilities but also independently certified by SGS, an external laboratory.

In addition, the design of the bolt was further improved by replacing the washer with a scalloped edge on the bolt head, reducing the risk of loss. This design change also resulted in fewer fasteners and washers being required during the assembly process, increasing productivity and reducing material costs. Most importantly, the new bolt provides an increased level of safety for cyclists, and its design seamlessly integrates into the simple, clean design of the BMC bike.

Highlights of the ecosyn® grip Bolt at a Glance

  • High anti-vibration capability
  • High fatigue-strength
  • Economical assembly
  • Savings on material costs
  • Awarded with the TAIPEI CYCLE Design & Innovation-Award

You have a project where you need design support?