Watch how our Engineering Team supported CWA in developing their new OMEGA V cabin.
Success Stories
Explore the development story of the OMEGA V cabin, where we supported CWA to find the optimal fasteners for critical connections. Together with our engineering services, this improved assembly speed, reduced parts, and optimized the assortment.

Watch how our Engineering Team supported CWA in developing their new OMEGA V cabin.

CWA Constructions SA/Corp. produces state-of-the-art cable car cabins and vehicles that impress both passengers and cable car operators alike. We at Bossard were also able to contribute and support the IMPACT project, which revolves around the new OMEGA V cabin. This cabin accommodates ten people and will be used in mountain regions as well as urban areas, from winter to summer. The first cabin was produced in the fall of 2018.
The first discussions about the development of the Omega V took place in 2016. Our engineers and CWA worked together closely from the very beginning. The timing was perfect as the cabin was in its early development stage. Efficient and safe solutions were sought for the new lightweight cabin.
Multi-functionality is a key word in the Omega V project. Many connections have to meet multiple requirements such as
Some of the most important connections in the cabin are the corner connections. The screws required for this are subjected to dynamic loads and are screwed into aluminum. In addition, there are high requirements for corrosion resistance.
Since a high level of safety is required in this project, we defined TAPTITE 2000® screws as the right product for the connections. 28 M10x70 of these thread-forming screws ensure the connection of the corner columns to the roof and floor frame.
A special zinc layer coating meets the requirements for corrosion resistance and lubrication. By using these multifunctional screws, combined with optimal design, the upstream thread-cutting and additional screw security are eliminated.
Another feature of the TAPTITE screws is that they comply with standard DIN 267-30 and thus meet all requirements of ISO 898-1 for strength class 10.9. In addition to these screws, thread-forming screws according to standard DIN 7500 were also used.
In the development process, the question arose of how to design a thread-forming screw for safety-relevant connections. The answer: with our Engineering Service Expert Design, we calculated and determined the dimensions based on the operating forces. The data of the tightening torque and preload force obtained were checked with various tests in our testing laboratory. In addition, the thread engagement depth was verified by over-torquing tests. The combination of the results yielded the dimensions for the design and the parameters for assembly.
In the course of development, a variety of surfaces, screw drives and materials accumulated. Together with CWA engineers, we examined the focus points of drives, surfaces and locking systems. In addition, we carried out an assortment analysis using our Expert Assortment Analysis Service.
Among numerous other improvements, DIN 7500 bolts were able to eliminate the need for additional locking elements. Blackened INOX fasteners meet the requirements for elegant design and hexagon socket drives (Torx) create the ideal conditions for partially or fully automated assembly.
To assemble TAPTITE 2000® thread-forming screws, an electrically driven screwdriver with torque and angle sensors is required. It should be noted that the screwdriver is additionally loaded with the so-called forming torque when using thread-forming screws. The screwing-in is carried out at high speed, whereby the tool switches to a slower speed before the head of the screw comes into contact, thus ensuring a process-safe tightening process. The Bossard engineering team accompanied the CWA assembly team during the assembly of the first cabins with the necessary tools and expertise.
The combination of our engineering services and the optimized multi-functional fasteners we provided resulted in the following advantages for CWA:
You have a project where you need comprehensive engineering support, too?