Hardness is generally the resistance of the material to penetration by a test body. There are different tests to determine the hardness of screws:
Vickers hardness HV: ISO 6507
Test body: pyramid (encompasses the complete hardness range usual for screws)
Brinell hardness HB: ISO 6506
Test body: ball
Rockwell hardness HRC: ISO 6508
Test body: cone
The advantage of the Vickers hardness test is that the entire hardness range encountered in the screw is covered by the method. For details, see ISO 898 Part 1.
Want to convert hardness values? Our online hardness conversion tool helps you convert hardness-to-hardness or hardness-to-tensile-strength values for unalloyed and low-alloy steels and cast iron.