Expert Test Services

Measurement of Coating Thickness in the Testing Laboratory

Coatings protect your components from the environment. To maintain this protection, coatings must have the appropriate thickness. Regular coating thickness analysis in a technical testing laboratory is advisable.

View inside the warehouse that contains semi-finished products, including various components of a cable car cabin.
ATE | Coating Thickness Measurement

Coating Thickness Measurement

Which coating you choose for your components depends on various factors, e.g: Which environment will the parts be used in?

Reliable processes are absolutely vital to ensure that your component won't face any harm. One of these processes is layer thickness measurement, which we carry out in our technical and accredited testing laboratories. Up to three layers on your metallic component are precisely measured with the aim of detecting any defects as early as possible, thus ensuring the quality of the components and their proper functioning.

Layer Thickness Measurement 101

The most suitable measurement method for assessing layer thickness in components typically depends on the base material and its coating. For instance, X-ray fluorescence (XRF) analysis is ideal for multi-coated metallic components, providing precise measurements of thicknesses and compositions. By exposing the sample to targeted X-rays, electrons are displaced within the atoms, emitting characteristic X-ray fluorescence radiation which experts measure to determine the thickness of up to three layers.

Bossard – Precise Metal Layer Thickness Measurement in the Testing Laboratory

Bossard uses X-ray fluorescence analysis in both accredited and standard testing laboratories. It is a non-destructive method that provides precise, targeted measurements of layer thickness despite the short time it takes.

In our test labs, we therefore test the required protective metal layer thicknesses of the following:

  1. components with up to three layers
  2. coatings consisting of zinc, nickel, chrome, zinc flake, gold, silver, and many more metals

Get Access to Bossard's Test Laboratory

As experts in fastening and materials technology, we conduct a wide range of tests in our technical laboratories to support your quality assurance.

Two men in a test lab examine a sewing machine on a desk in an industrial lab with additional workstations in the background. Key visual for Expert Test Services.

Contact Us for a Coating Thickness Measurement

Please complete the form. *fields are required.