Expert Test Services

Hardness Test – Determining Material Properties

Hardness testing is essential for ensuring material quality across various industries and in research and development. As an experienced partner, we support you with expertise and advanced test laboratories.

Close-up of hardness testing machine.

What Is a Hardness Test?

Hardness testing is a common procedure for determining the properties of a material. Hardness describes the resistance that a material puts up against a penetrating object. This makes it possible to test whether it is a hard and brittle material or one that is soft and tough or anything in between. This allows the tester to determine whether the tested material is suitable for a particular purpose.

Hardness testing is used in all kinds of different areas and sectors to ensure the required quality. The major industries where it is used include automotive, construction, aerospace, mechanical engineering, metal production and processing, and automation.

How a Hardness Test Works

The principle of hardness testing is relatively simple: An indenter, i.e., an object with a specific geometry, is pressed into the surface of the material to be tested with a certain force. This process creates an indentation, the dimensions of which the tester can measure. The hardness can then be calculated based on this measurement. The smaller the indentation, the harder the material being examined. The tester has a choice of various methods.

Vickers Hardness Test*

The Vickers hardness test is based on an optical measurement system. Testing according to the Vickers scale relies on a pyramidal diamond with a square base. The tester measures the length of both diagonals of the indentation left behind by the diamond. They then use the average value of the diagonals to calculate the hardness, with the hardness value and the test force always being mentioned together (e.g., 350 HV30). Because the indentation made by the diamond can be made very small, this measurement method is also suitable for small and very thin workpieces.

Rockwell Hardness Test*

The Rockwell hardness test (HRC) is performed using a diamond cone (120° point angle) to test the hardness of hardened steel. The tester first applies a preliminary force or a preliminary load to penetrate the surface of the material to be tested. After a certain dwell time, the base depth – which serves as a reference level and comes into play later when calculating the hardness – can be measured. The test force is then further increased to achieve the final penetration depth. After the dwell time, the test force is reduced again and the final penetration depth is measured. The tester then calculates the Rockwell hardness value based on the difference between the base depth and the final penetration depth. The final result of the hardness value combined with the test procedure represents the Rockwell hardness (e.g., 58HRC).

*Vickers hardness test accredited in Switzerland; Rockwell hardness test accredited in the U.S.

Hardness test in Bossard’s test labs

Contact us for hardness testing in our state-of-the-art laboratories. If you need certified tests, the Vickers hardness test is accredited in Switzerland and the Rockwell hardness test is accredited in the U.S. Please see certificates for details.

Get Access to Bossard's Test Laboratory

As experts in fastening and materials technology, we conduct a wide range of tests in our technical laboratories to support your quality assurance.

Two men in a test lab examine a sewing machine on a desk in an industrial lab with additional workstations in the background. Key visual for Expert Test Services.

Contact Us for a Hardness Test

Please complete the form. *fields are required.