Bossard SmartTools
Battery-powered screwdriving and riveting devices are the perfect start in digitalizing your production. Our Bossard SmartTools receive information about the next work step directly from the system and return information about the current work status. Configuration is simple and user-friendly. The tools can be operated in our work instructions software ELAM Solutions or stand-alone. They do not require an additional control system and can store 99 different screwdriving programs.
- Easy handling: All Bossard SmartTools are intuitive to use. New operators find their way quickly and easily and do not require long training periods.
- Direct status indication through colored LED: The fitter always receives immediate feedback from the tool through the LED display. The lights can be individually programmed and signal, for example, when the tool is is ready for use.
- Man-Machine-Communication: The OLED display shows all important information such as battery status, set torque, status of the last processing step and more. Settings for autonomous use of the tool can also be adjusted in the tool menu.
- Connected and Smart: The integrated WLAN module ensures wireless data transmission within the shop floor. The tools can be controlled with a central control software. The optional scanner can read 2D and bar codes and use this information to parameterize the machine for the next work step.